Hi,
I had JN5168 constantly powered for 2-3 months and functioning correctly as a ZigBee PRO router with some Home Automation cluster until recently.
Now I can see the chip starts to draws c.a. 300mA of current @ 3.3V as soon as I call ZPS_eAplAfInit() function. Until then the current is around 30mA. Interestingly the MCU functions correctly, I can program the chip and run the code. IO works ok too. I can see on the sniffer it transmits Beacon Requests but seems like it ignores the Beacons from coordinator (network discovery fails with MAC_ENUM_NO_BEACON). Also the internal temp sensor when read with ADC reads 0. So the symptoms really are
- 300mA of current consumption and chip getting quite warm (300mA x 3.3V = 1W)
- temp sensor or ADC not working
- receiver not working
I will reiterate that the device was working ok for 2-3 months 24/7. I suspect permanent damage to the IC.
So the question is: What can be the problem? What can be the route cause?
Regards,
Witek.
Hi,
I've disconnected all the components other then C, R and L specified in the datasheet and the problem remains. As soon as I call ZPS_eAplAfInit() the current draw goes high.
I did however desolder and resolder JN5168 and the problem went away what suggest one of the two:
1. There was some poor quality solder which got solved by resoldering
2. Treating the chip with 300C hotair "fixed" it's internal defect. Is it likely at all?
Hi Witold,
It looks that you damage the JN device.
Some suggestions to find out the root cause of this.
-Could you please remove components from your board? If some devices are consuming more current.
-Measure the pins of the JN if they are not in low impedance.
-What are the sensors that you have connected?
Regards,
Mario