1. RSSI do TOF on 25 channels, RSSI1 and RSSI2 send RSSI packets on channel 20.
Figure 1 Figure 2 is a close-up, occasional signal strength attenuation is particularly serious, and occasionally RSSI packet loss,
2.Figure 3 shows that large-area RSSI packet loss occurs at a distance of about 250m.
3.RSSI channel signal strength is always weaker than TOF channel signal strength
We don't know when this happened. The previous product did not have this situation and it needs to be solved.
Hi,
Are you working with the TOF? Time of Flight?
We do not recommend this module and is not supported.
What is the application that you trying to achieve, the RSSI value is not a value that you could take as reference, is not a constant because you will have a lot of noise in the environment.
Regards,
Mario
By the way what do you meaning “ you do not recommend this module and is not supported ”,and our Coordinator is JN5148
Hi,
As you know the JN5148 is no longer manufacture. It is not supported.
The JN5168 devices provided a TOF module, and also it is not supported.
Regards,
Mario
tks,We used the library files of the previous Jennic company, the TOF is no problem, the use process is normal, ok, let us forget the TOF, you can explain why the signal strength of the wireless signal frame sent by my END-Device broadcast is always Is floating, unstable
Hi,
The RSSI value is not always stable, it is not a constant. You will be affected by a lot of factors, environment, temperature, walls, other signals.
Regards,
Mario
Hi:
ok,The signal strength is not caused by changes in the external environment. Even if I put the two devices together, the signal strength value received by the Coordinator will jump or even be lost.
Maybe there is a problem with my code, let me check it again, and you have a routine to send wireless signals on a fixed channel. I can use sinffer to capture and view data. If so, please send me one. My email: limenglong@yiritech.com, thank you very much
Hi,
COuld you please look at the next link IEEE® 802.15.4 for JN516x and JN517x JN-AN-1172.
I can use sniffer to capture and view data
If you use the sniffer that value is from him not for the device.
Regards,
Mario