I have just started using a high powered JN5168-M05 for a project. Whilst it is running and sending out debug information the radio does not seem to be working at all. It does not link to a coordinator, and when it does an energy scan (as a coordinator) all the energies come back as 0.
I am using it in basic IEEE15.4 mode.
The same code works find on a M00 module.
I have called
vAppApiSetHighPowerMode( APP_API_MODULE_HPM05, TRUE ) before using radio.
I am using it with an external 2dB dipole antenna.
I have downloaded the NXP JN-AP-1172 JN516x Customer Module Evaluation Tool. I've compiled it in BeYond Studio with the latest SDK.
The results are similar : When I run it on a M00 and do the receive test or RF power measurement test I can see activity on the channels.
When I run the same binary (and enable high power mode from the terminal) on a M05 the channels are completely silent.
Its like the radio is not switched on in the M05.
I have tried two M05.
I have used the M00 module extensively without issue.
Antenna is not shorted or anything like that.
Has anyone got an M05 working? Any ideas what I could be doing wrong?
Thanks in advance for any help.
Solved! Go to Solution.
Ignore this - I was driving 5V into DIO1. It was configured as an input so but 5V is over voltage.
Calling the makers and experts interested in using Zigbee via NXP JN5168 modules, please join the facebook group so we can help each other:)
https://goo.gl/DeYbC6
Cheers
Hai,
I am also working on JN5168-001-M06. Can u plz tell me ho or where to get the beyond studio IDE and SDks.
I am really stuck. Plz help
Ignore this - I was driving 5V into DIO1. It was configured as an input so but 5V is over voltage.