Dear Sirs,
Using the ZGWUI to send On/Off/Toggle command to a Light-Bulb device, we can see the response message (ex: Type:0x8000 and others) showing on ZGWUI.
My questions are:
1. In which API of the Light-Bulb handling the response packet to Coordinator?
2. How to add a custom payload into the response packet for On/Off/Toggle command?
Thanks.
Solved! Go to Solution.
Dear Sirs,
Using the ZGWUI to send "Off " command (On/Off cluster) to a Light-Bulb device, we can see some message (as below) were printed in the "Received Message View" field of ZGWUI. Could you please show me which API of the Light-Bulb issue the response packet to the Gateway?
Type: 0x8101
(Default Response)
SQN: 0x10
Short Address: 0x6B9A
Source EndPoint: 0x00
Destination EndPoint: 0x00
Cluster ID: 0x0000 (General: Basic)
Command: 0x00
Status: 0x00
It seems issued from eZCL_SendDefaultResponse.