[JN-AN-1218] [Light Bulb] response for On/Off?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[JN-AN-1218] [Light Bulb] response for On/Off?

Jump to solution
806 Views
alan5_lin
Contributor III

Dear Sirs,

Using the ZGWUI to send On/Off/Toggle command to a Light-Bulb device, we can see the response message (ex: Type:0x8000 and others) showing on ZGWUI. 

My questions are:

1. In which API of the Light-Bulb handling the response packet to Coordinator?

2. How to add a custom payload into the response packet for On/Off/Toggle command?

Thanks.

0 Kudos
Reply
1 Solution
710 Views
alan5_lin
Contributor III

It seems issued from eZCL_SendDefaultResponse.

View solution in original post

0 Kudos
Reply
2 Replies
710 Views
alan5_lin
Contributor III

Dear Sirs,

Using the ZGWUI to send "Off " command (On/Off cluster) to a Light-Bulb device, we can see some message (as below) were printed in the "Received Message View" field of ZGWUI. Could you please show me which API of the Light-Bulb issue the response packet to the Gateway?   

  Type: 0x8101

  (Default Response)

  SQN: 0x10

  Short Address: 0x6B9A

  Source EndPoint: 0x00

  Destination EndPoint: 0x00

  Cluster ID: 0x0000 (General: Basic)

  Command: 0x00

  Status: 0x00

0 Kudos
Reply
711 Views
alan5_lin
Contributor III

It seems issued from eZCL_SendDefaultResponse.

0 Kudos
Reply