Hi
JN AN 1216_ ZigbeeNodeControlBridgeCoordinator_GP_Proxy cannot receive green power.
It is received before starting the Start Network. (APP_vControlNodeStartNetwork() )
Once the network is created, green power cannot be received.
how do i solve it ?
If it is set to sBDB.sAttrib.u8bdbCommissioningMode = 0;
and network creation fails, green power is received.
thanks
已解决! 转到解答。
Hi mario,
When I double-checked to provide the log, it turned out to be successful.
thanks
Regards,
seungho
Hi @seunghokims,
I hope you are doing great.
Just to confirm, did you define the Green power support in the makefile?
GP_SUPPORT = 1
Regards,
Mario
Hi Mario
Yes
I defined GP_SUPPORT = 1 .
so
After setting the Zigbee Node Control Bridge Coordinator channel,
Receive green power data generated from JN-AN 1219 EH_Switch.
--> After running Start Network in Zigbee Node Control Bridge Coordinator
Cannot receive green power data.
It is received before starting the Start Network.
how do i solve it
Regards,
Hi @seunghokims,
Is it possible that you could provide the sniffer log of this issue?
Also, is it possible that you could provide the terminal log for the devices that you have?
Regards,
Mario