Hi
JN AN 1216_ ZigbeeNodeControlBridgeCoordinator_GP_Proxy cannot receive green power.
It is received before starting the Start Network. (APP_vControlNodeStartNetwork() )
Once the network is created, green power cannot be received.
how do i solve it ?
If it is set to sBDB.sAttrib.u8bdbCommissioningMode = 0;
and network creation fails, green power is received.
thanks
解決済! 解決策の投稿を見る。
Hi mario,
When I double-checked to provide the log, it turned out to be successful.
thanks
Regards,
seungho
Hi @seunghokims,
I hope you are doing great.
Just to confirm, did you define the Green power support in the makefile?
GP_SUPPORT = 1
Regards,
Mario
Hi Mario
Yes
I defined GP_SUPPORT = 1 .
so
After setting the Zigbee Node Control Bridge Coordinator channel,
Receive green power data generated from JN-AN 1219 EH_Switch.
--> After running Start Network in Zigbee Node Control Bridge Coordinator
Cannot receive green power data.
It is received before starting the Start Network.
how do i solve it
Regards,
Hi @seunghokims,
Is it possible that you could provide the sniffer log of this issue?
Also, is it possible that you could provide the terminal log for the devices that you have?
Regards,
Mario
Hi mario,
When I double-checked to provide the log, it turned out to be successful.
thanks
Regards,
seungho