As in the subject line. While there is a good set of documentation on Thread Stack, I can find nothing on nwk_ip.
I am very skeptical of your Thread Stack implementation if it depends upon functions in nwk_ip - it is seems as if the Thread Stack API is tightly coupled to what is in the nwk_ip. I sincerely hope that I am wrong.
Example: The pointer to the function Stack_to_APP_Handler in router_eligible_device_app.c is in a array of structures of type eventManagerEntry_t called aStaticEventsTable[], BUT there is no real documentation whatsoever on this, and I am left with the assumption that a library in nwk_ip must reference it.
Please provide information on this as soon as possible.
Thanks,
George Wicks
Hi George,
Unfortunately the only documentation available is Kinetis Thread Stack Application Development Guide and you can find it following the next path.(Connectivity Software 1.0.2)
C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\Thread
Best Regards,
Mario