Is it require to add cluster in router device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it require to add cluster in router device?

ソリューションへジャンプ
1,484件の閲覧回数
bhautik_ruparel
Contributor II

Hello Support Team,

I have used one Coordinator, Router and End device and configured cluster on Coordinator and End device side as per application.

I configure Dimmable Light [0x0101] as a router.

So Is it require to add/configure cluster [i.e. Group, Scenes, Level Control, On/Off cluster, etc.] on router side? 

Regards,

Bhautik

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
1,417件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @bhautik_ruparel,

In this case, the router will be sent the packet to the coordinator, if the destination address is the coordinator, but you are right the router doesn't need any cluster for this.

Regards,

Mario

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,418件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @bhautik_ruparel,

In this case, the router will be sent the packet to the coordinator, if the destination address is the coordinator, but you are right the router doesn't need any cluster for this.

Regards,

Mario

0 件の賞賛
返信
1,442件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @bhautik_ruparel,

In this case, if you do not add this cluster functionality, the router can not respond and support some commands that the coordinator could request. It will depend on your application

Regards,

Mario

0 件の賞賛
返信
1,432件の閲覧回数
bhautik_ruparel
Contributor II

Hello @mario_castaneda 

Thanks for your response.

As per our application I have configure router [Dimmable Light] as a range extender and also just routing the packet from end device to coordinator and vice versa. 

So In this condition no need to require to add or configure cluster. Is that my understanding right?

Regards,

Bhautik 

0 件の賞賛
返信