Hello,
I have seen JN-AN-1175-JN516x-Packet-Error-Rate-Tool for PER test for SE profile and Started communication between AN1175_PER_TTY_Master and AN1175_PER_Slave Application on JN5168 chip.
On AN1175_PER_TTY_Master Application SIde
I give below details on CLI.
Options
>Channel: 11
Power Mode: Low
Power Level: 24
Retries: 3
LEDs: Disabled
Done
Up(1) Down(2) Select(3)
I got result on ACK mode
Channel 11
Mode Ack
Seen 0
Total 3322
PER % 100.0
CCA Fail % 0.0
Retries 3
LQI 0
Chan (1) Stop (2) Mode (3)
I need to add RSSI Field in this Application. How to calculate RSSI or which APIs is used?.
Do you know anyone ?,If yes,please put the steps or details.
已解决! 转到解答。
Since you are using JPT, you can have a look at:
C:\NXP\bstudio_nxp\sdk\JN-SW-4163\Components\ProductionTestApi\Include\jpt.h
or
C:\NXP\bstudio_nxp\sdk\*SDK NUMBER*\Components\ProductionTestApi\Include\jpt.h
for more API commands.
If you would have a look at JN-DS-JN516x.pdf, page 29, there is a graph charting LQI vs dBm.
At AN1175_PER_TTY_Master.c, you can intercept line 537 then add your own "convert the LQI to dBm/RSSI" function.
Offtopic:
If you just want to do some range testing, I would recommend using this: JN-AN-1172-JN516x-Customer-Module-Evaluation-Tool
It's more detailed & configurable (testing-wise) in my opinion.
Since you are using JPT, you can have a look at:
C:\NXP\bstudio_nxp\sdk\JN-SW-4163\Components\ProductionTestApi\Include\jpt.h
or
C:\NXP\bstudio_nxp\sdk\*SDK NUMBER*\Components\ProductionTestApi\Include\jpt.h
for more API commands.
If you would have a look at JN-DS-JN516x.pdf, page 29, there is a graph charting LQI vs dBm.
At AN1175_PER_TTY_Master.c, you can intercept line 537 then add your own "convert the LQI to dBm/RSSI" function.
Offtopic:
If you just want to do some range testing, I would recommend using this: JN-AN-1172-JN516x-Customer-Module-Evaluation-Tool
It's more detailed & configurable (testing-wise) in my opinion.
Hello,
I will be using this JN-AN-1172-JN516x-Customer-Module-Evaluation-Tool application .Do you know the transmit power mode for JN5168 and JN5169. if you know and have any documents,please provide me.