Hello
Previously a representative told me MKW24D supports both ZigBee and Thread. This is not a special case for 24D right? 21D can also support ZigBee and Thread simultaneously? Can you confirm this.
Also what are the advantages of Smart Energy 2.0 in a nutshell? What are the advantages of having FlexRAM and FlexNVM? From what I understand of AN4282, it simply means you can partition some of your RAM and Flash to be used as an EEPROM. I get the RAM part but why would I want to partition my Flash as an EEPROM? Any use cases you can think of or can give examples about. Am I misinterpreting?
Regards,
Mete
Solved! Go to Solution.
Hello Atilla,
As you can see in the Thread Release notes, the KW21D device only is supported as end device.
The memory footprint will be your main constrain so I recommend you to take a look into this topic.
The Thread Release notes also show some memory recommendations that could give you a clue about it.
Best regards,
Earl.
Hello Atilla,
As you can see in the Thread Release notes, the KW21D device only is supported as end device.
The memory footprint will be your main constrain so I recommend you to take a look into this topic.
The Thread Release notes also show some memory recommendations that could give you a clue about it.
Best regards,
Earl.
Hi Mete,
I'm not expert on your topic but have several links to help with FlexRAM/FlexNVM and Smart Energy 2.0.
Hope others help with your remaining questions.
Regards,
David