Hiii ,
I am using AT45DB041E flash which are available on FRDM-KW41Z evaluation borad ,
Interfacing of AT45DB041E using SPI communication , using this Read Manufacturer ID and Device ID successfully , but for read data it always read FF or 00
unsigned char RdFlashByte(unsigned int BuffAddr)
{
unsigned char rddata = 0 ;
unsigned char t1[5]={0};
PRINTF("\nRdFlashByte\r\n");
while(!FlashReadBusy()); //wait if device is busy
t1[0] = BUFFER_1_READ; //or 0xD1
t1[1] = 0x00;
t1[2] = ((unsigned char)(BuffAddr>>8));
t1[3] = ((unsigned char)(BuffAddr));
t1[4] = 0x00;
isTransferCompleted = false ;
dspi_transfer_t masterXfer;
masterXfer.txData = &t1[0] ;
masterXfer.rxData = NULL ;
masterXfer.dataSize = 5 ;
masterXfer.configFlags = kDSPI_MasterCtar1 | EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER | kDSPI_MasterPcsContinuous;
DSPI_MasterTransferNonBlocking(EXAMPLE_DSPI_MASTER_BASEADDR, &g_m_handle, &masterXfer);
/* Wait transfer complete */
while (!isTransferCompleted)
{
}
/* Delay to wait slave is ready */
for (i = 0; i < EXAMPLE_DSPI_DEALY_COUNT; i++)
{
__NOP();
}
isTransferCompleted = false ;
masterXfer.txData = NULL ;
masterXfer.rxData = &rddata ;
masterXfer.dataSize = 1 ;
masterXfer.configFlags = kDSPI_MasterCtar1 | EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER | kDSPI_MasterActiveAfterTransfer;
DSPI_MasterTransferNonBlocking(EXAMPLE_DSPI_MASTER_BASEADDR, &g_m_handle, &masterXfer);
/* Wait transfer complete */
while (!isTransferCompleted)
{
}
/* Delay to wait slave is ready */
for (i = 0; i < EXAMPLE_DSPI_DEALY_COUNT; i++)
{
__NOP();
}
PRINTF("\n Rx data :%d \r\n,",rddata);
return rddata;
} //End of RdFlashByte Function
please give some idea.
Hello,
As I do not have the same memory as you do, I'm limited to the capabilities of the device and my available resources which are from NXP and our developments boards.
How are you confirming that you are reading and writing correctly form the memory? Are you checking the registers with the received data?
Regards,
Estephania
Hello,
Are you basing it on an example? If you are, could you please let me know if you are, could you please give me more details about it?
Also, are you having some kind of fault? Or is it just that it is not reading the correct value?
Regards,
Estephania