c:/nxp/bstudio_nxp/sdk/tools/ba-elf-ba2-r36379/bin/../lib/gcc/ba-elf/4.7.4/../../../../ba-elf/bin/ld.exe: cannot open linker script file AppBuildZBPro.ld: No such file or directory
The file AppBuildZBPro.ld is not in the sources nor in the SDK. How could I workaround this error?
Please help.
Thanks
LM
Yes, I have installed that SDK.
I managed to finish the linking process by editing the /build/Makefile.
It appears that in the original Makefile, there is a commented line just before the reference to AppBuildZBPro.ld.
This show me that there were other linker scripts files e.g. AppBuildZBPro_JN5169.ld.
I replaced AppBuildZBPro.ld by AppBuildZBPro_JN5169.ld inside the Makefile and voilà.
But now my problem is that the debug traces are not displayed on my serial terminal. But this is another issue.
Hi Louis,
Did you define the debug port for the UART0? Are you using JTAG?
http://www.nxp.com/documents/application_note/JN-AN-1203.pdf?fsrch=1&sr=6&pageNum=1
4.2.1
Hope it helps.
Best Regards,
Mario
Have you installed the ZigBee SDK (JN-SW-4168)?