Hi All,
I'm developing ZB30 application for JN5179, and want to use ZPS configuration editor as JN-UG-3113 described - to found it under "Jennic option". But I cannot find it in "LPCXpresso_7.9.2_493"
I have installed the newest JN-SW-4263 and 4270 as below.
Can you make a suggestion where is the problem? Thanks!
In "JN-RN-0062-JN-SW-4270-JN517x-ZigBee3-SDK.pdf" (v1520) says:
Software Component contains "ZPS Configuration Plug-ins [v31504]". So where can we find it?
Thank you,
Benjamin
Hi Benajmin,
-Please follow the path Help > Install New Software….
-In the Available Software screen, click the Add… button. The following Add Respository window will be displayed.
-In the Add Repository window:
-In the Available Software screen, expand Jennic ZBPro SDK and ensure that the checkboxes for Jennic RTOS Configuration Editor and Jennic ZBPro Configuration Editor are ticked. Click Next > to continue
-Continue following the step 6
1.2.3 Installing the ZigBee Plug-ins
http://www.nxp.com/documents/user_manual/JN-UG-3098.pdf?fsrch=1&sr=1&pageNum=1
Hope it helps,
Mario
Hello Mario,
It works and got as below wizard. Thank you!
It is the same procedure as Danny described in Section 1.2.2 of JN-UG-3109.
Just wondering why my previous installation of JN-SW-4270 did not include this? I rember to have followed Section 3.2 "SDK Plug-in Installation" of "JN-RN-0062-JN-SW-4270-JN517x-ZigBee3-SDK.pdf", but only to found "All items are installed" message displayed under "NXP RFCS JN-SW-4270 Software Development Kit".
Thank you,
Benjamin
Hi Benjamin,
*EDITED - Wrong Document. Below is now correct*
Please following the document below at section 1.2.2
http://www.nxp.com/documents/user_manual/JN-UG-3109.pdf
Danny.