When I build the "JN-AN-1218-Zigbee-3-0-Light-Bulb" In BeyondStudio for NXP. Some of these problems arise:
Sdk: JN-SW-4170
Chip:JN5169
How can i fix it ?
下载最新 的版本号。可以解决此问题
Hi, I have the same issue.
I'm using JN 5179 and LPCXpresso
I installed Plugins.
I followed "MENP-JN5179_Firmware_Build_Guide", but it appear these error. What wrong with my program?
Hi Vu Luu,
What is the application note that you are working on? version? Did you compile or program another example before?
I want to be sure plugins are not the problem.
Mario
Hi Mario,
I'm working MENP-JN5179-RGB Click in "JN-AN-1218-Zigbee-3-0-Light-Bulb" version 1002 but all configuration of this version have same error like that picture. I also try to compile some configuration in version 1006 and it's successfully. But it doesn't have MENP-JN5179-RGB Click. Do you have any example about MENP-JN5179 RGB Click? I'm using SDK "JN-SW-4270-ZigBee-3.0-v1746"
Hi Vu Luu,
Could you please download the version 1006?
Note: The JN5179 has limited support.
Mario
Hi Mario,
Yes, version 1006 is working, but it's not include MENP-RGBClick Board. I have a MENP board and I want to control it.
Are there any example about it?
Here is an error in version 1002.
Hi Vu Luu,
Please take as reference the next document https://community.nxp.com/docs/DOC-340127
The JN-AN-1218 version 1002 requires some changes to be compatible with the v1746 version.
Note: The changes that the AN needs, are not in the same .c or .h file like the AN mentions.
Mario
Hi Mario,
I can't find the same file in JN-AN-1218. As I know, JN-AN-1218 ver 1002 is based on the SDK ver 1520. Do you have SDK version 1520? Please send to me the link to download it.
Hi,
I clean and compile it, the dimmable light examples.
SDK: JN-SW-4170 v1735
AN: JN-AN-1218 V1005
What is the version that you are using?
Regards,
Mario
I can't find the version you said on the NXP website.
Oh! I got it, Thank you very much!
SDK: JN-SW-4170 v1731
AN: JN-AN-1218 V1003