Build "JN-AN-1218-Zigbee-3-0-Light-Bulb" err

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build "JN-AN-1218-Zigbee-3-0-Light-Bulb" err

2,429 Views
mingmo
Contributor II

When I build the "JN-AN-1218-Zigbee-3-0-Light-Bulb" In BeyondStudio for NXP. Some of these problems arise:

pastedImage_1.png

Sdk: JN-SW-4170

Chip:JN5169

How can i fix it ?

Labels (1)
0 Kudos
13 Replies

1,559 Views
行军程
Contributor II

下载最新 的版本号。可以解决此问题

1,559 Views
vuluu
Contributor II

Hi, I have the same issue.

I'm using JN 5179 and LPCXpresso

I installed Plugins.

Capture.PNG

2.PNG

I followed "MENP-JN5179_Firmware_Build_Guide", but it appear these error. What wrong with my program?

0 Kudos

1,559 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vu Luu,

What is the application note that you are working on? version? Did you compile or program another example before?

I want to be sure plugins are not the problem.

Mario

0 Kudos

1,559 Views
vuluu
Contributor II

Hi Mario,

I'm working MENP-JN5179-RGB Click in "JN-AN-1218-Zigbee-3-0-Light-Bulb" version 1002  but all configuration of this version have same error like that picture. I also try to compile some configuration in version 1006 and it's successfully. But it doesn't have MENP-JN5179-RGB Click. Do you have any example about MENP-JN5179 RGB Click? I'm using SDK "JN-SW-4270-ZigBee-3.0-v1746"

0 Kudos

1,559 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vu Luu,

Could you please download the version 1006?

Zigbee3.0

Note: The JN5179 has limited support.

Mario

0 Kudos

1,559 Views
vuluu
Contributor II

Hi Mario,

Yes, version 1006 is working, but it's not include MENP-RGBClick Board. I have a MENP board and I want to control it.

Are there any example about it?

Here is an error in version 1002. Untitled.png

0 Kudos

1,559 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vu Luu,

Please take as reference the next document https://community.nxp.com/docs/DOC-340127 

The JN-AN-1218 version 1002 requires some changes to be compatible with the v1746 version. 

Note: The changes that the AN needs, are not in the same .c or .h file like the AN mentions.

Mario

0 Kudos

1,559 Views
vuluu
Contributor II

Hi Mario,

I can't find the same file in JN-AN-1218. As I know, JN-AN-1218 ver 1002 is based on the SDK ver 1520. Do you have SDK version 1520? Please send  to me the link to download it.

0 Kudos

1,559 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I clean and compile it, the dimmable light examples.

SDK: JN-SW-4170 v1735 

AN: JN-AN-1218 V1005

pastedImage_1.png

What is the version that you are using? 

Regards,

Mario

0 Kudos

1,559 Views
mingmo
Contributor II

I can't find the version you said on the NXP website.

0 Kudos

1,559 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ming,

Please follow the next link

ZigBee 3.0|NXP 

pastedImage_2.png

Regards,

Mario

1,559 Views
mingmo
Contributor II

Oh! I got it,  Thank you very much!

0 Kudos

1,559 Views
mingmo
Contributor II

SDK: JN-SW-4170 v1731

AN: JN-AN-1218 V1003

0 Kudos