Bluetooth,IEEE 802.15.4,SMAC,Thread

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth,IEEE 802.15.4,SMAC,Thread

1,488件の閲覧回数
bjemt
Contributor III

KW41Z support BLE and IEEE 802.15.4 ,  MKW41Z_ConnSw_1. 0.2 wireless sample Divided into Bluetooth, IEEE 802.15.4, SMAC, Thread agreements. In the NXP community is also divided into the four categories.

Where I can find the content to introduces the performance and characteristics  on these four agreements?

If my equipment directly connect to the laptop or the PAD over its bluetooth devices, Is the equipment must use the BLE protocol stack?

1 返信

1,040件の閲覧回数
jc_pacheco
NXP Employee
NXP Employee

Hello, 

Please refer to each stack's release notes documentation available in the docs folder.

C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\SMAC

C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\IEEE 802.15.4

C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\GENFSK

C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\Thread

C:\NXP\MKW41Z_ConnSw_1.0.2\docs\wireless\Bluetooth

If you want to connect a Bluetooth Low Energy device to your board, you must load the BLE stack into your board.

I'd recommend you to go through the FRDM-KW41Z|Freedom Development Kit|NXP  --> Getting Started tab.

-JC