Using the 88W8977 BLE+Wifi chip I'm trying to understand how long the device can stay powered while advertising (as a BLE peripheral) using battery power.
In the datasheet there is a current consumption table which has:
Bluetooth LE advertise(interval=1.28s): 0.047mA @ 1.8V.
(With Wifi in deep sleep mode).
Is the value (0.047mA) the average current draw? so the battery life is simply:
Battery Life = Battery Capacity (mAH) / 0.047mA. (Assuming a 1.8V battery?).
example: Battery Life = 2500 mAH / 0.047mA --> 53,191 hours or 6.07 years
I understand this life is only accurate if the device does nothing else which isn't realistic, but I want to know if I understand the chart correctly.
Thanks!
已解决! 转到解答。
Hi @danf,
You are right it is the average in this scenario, but you have to be aware of the Current consumption during
device initialization, the modules that you will have enabled WIFI, etc.
Regards,
Mario
Hi @danf,
You are right it is the average in this scenario, but you have to be aware of the Current consumption during
device initialization, the modules that you will have enabled WIFI, etc.
Regards,
Mario