Battery life computation during BLE advertising

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Battery life computation during BLE advertising

跳至解决方案
948 次查看
danf
Contributor II

Using the 88W8977 BLE+Wifi chip I'm trying to understand how long the device can stay powered while advertising (as a BLE peripheral) using battery power.

In the datasheet there is a current consumption table which has:

Bluetooth LE advertise(interval=1.28s): 0.047mA @ 1.8V.

(With Wifi in deep sleep mode).

Is the value (0.047mA) the average current draw? so the battery life is simply:

Battery Life = Battery Capacity (mAH) / 0.047mA. (Assuming a 1.8V battery?).

example: Battery Life = 2500 mAH / 0.047mA --> 53,191 hours or 6.07 years

I understand this life is only accurate if the device does nothing else which isn't realistic, but I want to know if I understand the chart correctly.

Thanks!

 

0 项奖励
1 解答
939 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @danf,

You are right it is the average in this scenario, but you have to be aware of the Current consumption during
device initialization, the modules that you will have enabled WIFI, etc. 

Regards,

Mario

在原帖中查看解决方案

0 项奖励
2 回复数
935 次查看
danf
Contributor II

Thanks! That makes sense. I appreciate your help!

0 项奖励
940 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @danf,

You are right it is the average in this scenario, but you have to be aware of the Current consumption during
device initialization, the modules that you will have enabled WIFI, etc. 

Regards,

Mario

0 项奖励