88w9098 - how to individually select on/off either WiFi or Bluetooth.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

88w9098 - how to individually select on/off either WiFi or Bluetooth.

ソリューションへジャンプ
2,284件の閲覧回数
isyu
Contributor III

Hello, 

About the NXP WIFI/BT Combo products, especially 88W9098> 

Is it possible to independently turn on/off WIFI and BT in both H/W and S/W?

How to individually select on/off either WiFi or Bluetooth.

1) During individual off of WiFi/BT, the current consumption value should also be reduced as much as the off portion.

2) Please check if there is a way to independently turn on/off WIFI and BT in both H/W and S/W.

Regards/I.S

ラベル(3)
0 件の賞賛
返信
1 解決策
2,249件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi @isyu 

 

WiFi & BT does not support independent Power Down and Power On.

 

Have a good day!

Regards,

weidong

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,250件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi @isyu 

 

WiFi & BT does not support independent Power Down and Power On.

 

Have a good day!

Regards,

weidong

0 件の賞賛
返信
2,246件の閲覧回数
isyu
Contributor III

Hello Weidong, 

Always thank you for your support. 

Well understood. 

I have one more question about power consumption. 

Actually, my customer will not use the WiFi function so often, just mainly use the BT function in his mobile printer.

In this case, to get the lowest power consumption, should I unload the wifi module/FW  or just go sleep mode ? which one is the better option?

Regards,

I.S

0 件の賞賛
返信
2,231件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @isyu ,

 

You can only use Bluetooth firmware , not use combo version.

 

Regards,

weidong

0 件の賞賛
返信
2,227件の閲覧回数
isyu
Contributor III

Hello @weidong_sun ,

Thank you for your answer. 

Yes, for individual usage on WiFi and BT, I will use BT firmware and WiFi firmware individually, will not use the combo version. 

My question was which one uses the lower power consumption between the power save mode in WiFi and unloading the WiFi driver/FW. 

In my understanding, unloading the WiFi driver/FW is a better solution. Am I correct?

I have one more question about power consumption. 

Actually, my customer will not use the WiFi function so often, just mainly use the BT function in his mobile printer.

In this case, to get the lowest power consumption, should I unload the wifi module/FW  or just go sleep mode ? which one is the better option?

Regards,

I.S

0 件の賞賛
返信
2,219件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @isyu ,

 

>>In my understanding, unloading the WiFi driver/FW is a better solution. Am I correct?

>>Actually, my customer will not use the WiFi function so often, just mainly use the BT function in his mobile printer.

According to above description, the customer will not use the WiFi function so often, it means that there still exists possiblity for her to use WiFi , so I suggest that she had better use combo version of firmware.

when using wifi, she only needs to let it up, if not, let it down.

 

Have a good day!

Regards,

weidong

0 件の賞賛
返信
2,282件の閲覧回数
isyu
Contributor III

In the 88W9098, I can find the below information regarding Power Management. 

Power management
Low-power dissipation
Integrated Buck regulator for core power supply
Sleep and standby modes for low-power operation
Separate power island for independent enable/disable of Bluetooth radio

It seems that the WIFI and BT block power can be controlled independently. 

But there's only one Power Down pin in Hardware (PDn). 

(there are no separate WIFI Power-Down and BT Power-Down Pin) 

 

0 件の賞賛
返信