88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen

23,064 Views
yao_feng
Contributor III

The FW crashed issue is still exist in Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL.

follow previous case:

https://community.nxp.com/t5/Wireless-Connectivity/88W8997-module-command-timeout-issue-interface-PC...

and reopen by this case.  

@ArthurC
@Christine_Li
88W8997 

0 Kudos
Reply
169 Replies

8,017 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

Can you please help to provide the dmesg+ fw_dump +drv_dump logs based on the new release?

Please pay attention to the parameter: drvdbg = 0xa0037​ when load drivers and make sure FW dump is available. After issue is occurred, directly export the logs without rebooting your device. Once device is reboot, FW dump will be lost.

Also do not use below command before export the failed logs because below command will automatically trigger another FW dump and it will override the real failed one.

echo debug_dump > /proc/mwlan/adapter0/config 

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

7,983 Views
ArthurC
Contributor III

Hello @Christine_Li

 

On waiting the official release about Wi-Fi FW crashing issue fixed.

0 Kudos
Reply

7,976 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @ArthurC 

Thanks for your reply.

I am checking with our internal team, will share with you once have any updates.

 

Best regards,

Christine.

0 Kudos
Reply

8,011 Views
yao_feng
Contributor III

Hi @ArthurC 
Could you please help to share with NXP:

dmesg
fw_dump
drv_dump

based on new release.
parameter settings: drvdbg = 0xa0037

After issue is occurred, directly export the logs without rebooting your device. Once device is reboot, FW dump will be lost.

!!! Don't do below before export logs. it will overwrite the old one.

echo debug_dump > /proc/mwlan/adapter0/config 

 

Thank you very much.

0 Kudos
Reply

7,937 Views
ArthurC
Contributor III

Hello @yao_feng ,

 

During the test thease days as 88W8997 Wi-Fi driver probing with parameter "drvdbg = 0xa0037"

 

We found the FW Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL which will cause host system hanging & crashed.

So we can't dump the internal logs by following command.

echo debug_dump > /proc/mwlan/adapter0/config 

 

What's the power consumption about the module 88W8997 caused by FW Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL ?

 

The dmesg about driver probed with parameter "drvdbg = 0xa0037" from start to host system hanging & crashed is as attached.

Please to analysis and fix issue.

 

0 Kudos
Reply

7,931 Views
yao_feng
Contributor III

Hi @ArthurC 
Please help to share your bring up commands.
for the current log, there is no WiFi FW hang message.

Thanks.

Tags (1)
0 Kudos
Reply

7,926 Views
ArthurC
Contributor III

Hello @yao_feng ,

The bring-up command:

modprobe moal mod_para=nxp/wifi_mod_para.conf drvdbg=0xa0037

There is no WiFi FW hang message because the whole system have been hang by the module 88W8997 with FW Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL.

Worse than previous version!


That's the current final dmesg log record to the log file stored to EMMC.

It's caused every time in 2.4G WiFi connection.

 

 

0 Kudos
Reply

7,917 Views
yao_feng
Contributor III

Hi @ArthurC 
could you please help to try modprobe moal mod_para=nxp/wifi_mod_para.conf

without debug level setting, check if it still have system hang issue or not.

and please share wifi_mod_para.conf with us.

Thanks. 


Tags (1)
0 Kudos
Reply

7,899 Views
ArthurC
Contributor III

Hello @yao_feng,

 

Without debug level setting, it's on working but the 88W8997 will be caused FW crashing.

 

Our used wifi_mod_para.conf is as attached.

0 Kudos
Reply

7,888 Views
yao_feng
Contributor III

Hi @Christine_Li 

drvdbg=0xa0037 seems cause system hang and can't test normally, any suggestion or other settings is ok for FW dump correctly?

The driver parameters settings are below
Please help to review if its ok?

PCIE8997 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=1
auto_ds=1
host_mlme=1
fw_name=nxp/pcie8997_wlan_v4.bin
sta_name=wlan
drv_mode=3
}

Thanks.

0 Kudos
Reply

7,831 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @ArthurC 

Can you please have a try with drvdbg=0x20037?

At the same time, I will double confirm with our internal team whether Q1-24 release surely include the fix of this issue as promised before. 

Best regards,

Christine.

0 Kudos
Reply

7,823 Views
ArthurC
Contributor III

Hello @Christine_Li,

 

Yes, I have tried for 10 times.

The FW with drvdbg=0x20037 in 2.4G connection caused whole system hang everytimes.

0 Kudos
Reply

7,817 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @ArthurC 

So for both drvdbg=0x20037 and drvdbg=0xa0037,  in 2.4G connection , will cause whole system hang every time. But without drvdbg parameter, system will not hang but still have FW crash.

Am I right?

Best regards,

Christine.

0 Kudos
Reply

7,794 Views
ArthurC
Contributor III

Hello @Christine_Li ,

 

The FW crashed dmesg log about probe without both drvdbg=0x20037 and drvdbg=0xa0037 is as attached.

0 Kudos
Reply

7,811 Views
ArthurC
Contributor III

Hello @Christine_Li ,

 

Yes, thank you.

0 Kudos
Reply

7,805 Views
yao_feng
Contributor III

Hi @ArthurC 

Could you please help to try

1. Replace FW to combo one: pcieuart8997_combo_v4.bin with drvdbg=0xa0037

2. Set
ps_mode=2
auto_ds=2

with drvdbg=0xa0037

= = =
in my experience, drvdbg level will not cause system hang, did you upgrade i.MX8 image or not?

0 Kudos
Reply

6,681 Views
ArthurC
Contributor III

Hello @yao_feng ,

 

With pcieuart8997_combo_v4.bin, the default uart speed is 115200.

It is out of our requirement about audio play via A2DP.

As we known, if we need Bluetooth uart working in baud 3M. 

There are flows including killing hciattach. 

It's not OK for production.

So we will not use pcieuart8997_combo_v4.bin.

 

0 Kudos
Reply

6,495 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @ArthurC 

Thanks for your logs and information.

I checked internally about this release, our internal team mentioned they have raised a JIRA ticket and fixes have been merged. So it might be a new issue because of some other submits.

According to the given logs, we will continue to track.

Also about the issue that drvdbg=0x20037 and  drvdbg=0xa0037 will cause system hang, I will report internally and may try to reproduce locally.

Once have any feedback, I will sync with you at the first time.

 

Best regards,

Christine.

0 Kudos
Reply

6,438 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @ArthurC 

May I ask about the issue that drvdbg=0x20037 and  drvdbg=0xa0037 will cause system hang, need to start iperf in STA mode connect with 2.4G AP and Bluetooth Audio at the same time then can reproduce?

About how long this issue will happen on your side?

I am setting up the environment to reproduce this issue.

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

6,423 Views
ArthurC
Contributor III

Hello @Christine_Li

May I ask about the issue that drvdbg=0x20037 and  drvdbg=0xa0037 will cause system hang, need to start iperf in STA mode connect with 2.4G AP and Bluetooth Audio at the same time then can reproduce?

-> Yes, BTW, please use Bluetooth uart working in baud 3M, first.

About how long this issue will happen on your side?

-> After 5 minutes.

 

Thank you for your help.

 

0 Kudos
Reply