Platform (Host CPU): i.MX8MQ
Wi-Fi module: AW-CM276NF (interface PCIE/UART)
OS: Linux
[ 4.909207] mwifiex_pcie 0000:01:00.0: no quirks enabled
[ 4.909234] mwifiex_pcie 0000:01:00.0: enabling device (0000 -> 0002)
[ 4.909326] mwifiex_pcie: PCI memory map Virt0: 0000000024acaf60 PCI memory map Virt2: 00000000050d867e
[ 5.555157] mwifiex_pcie 0000:01:00.0: info: FW download over, size 439256 bytes
[ 6.313354] mwifiex_pcie 0000:01:00.0: WLAN FW is active
[ 6.349480] mwifiex_pcie 0000:01:00.0: Unknown api_id: 5
[ 6.359375] mwifiex_pcie 0000:01:00.0: info: MWIFIEX VERSION: mwifiex 1.0 (16.92.21.p84)
[ 6.359393] mwifiex_pcie 0000:01:00.0: driver_version = mwifiex 1.0 (16.92.21.p84)
WiFi iperf test:
iperf3 –c 133.33.33.13 –t 86400
Audio play via bluealsa
aplay –D bluealsa:< BT MAC> xxx.wav
dmesg with FW coredump:
[30166.238363] mwifiex_pcie 0000:01:00.0: mwifiex_cmd_timeout_func: Timeout cmd id = 0xa4, act = 0x0
[30166.247313] mwifiex_pcie 0000:01:00.0: num_data_h2c_failure = 0
[30166.253280] mwifiex_pcie 0000:01:00.0: num_cmd_h2c_failure = 0
[30166.259137] mwifiex_pcie 0000:01:00.0: is_cmd_timedout = 1
[30166.264644] mwifiex_pcie 0000:01:00.0: num_tx_timeout = 0
[30166.270067] mwifiex_pcie 0000:01:00.0: last_cmd_index = 1
[30166.275480] mwifiex_pcie 0000:01:00.0: last_cmd_id: 16 00 a4 00 16 00 a4 00 7f 00
[30166.282984] mwifiex_pcie 0000:01:00.0: last_cmd_act: 00 00 00 00 00 00 00 00 00 00
[30166.290579] mwifiex_pcie 0000:01:00.0: last_cmd_resp_index = 0
[30166.296434] mwifiex_pcie 0000:01:00.0: last_cmd_resp_id: 16 80 7f 80 16 80 a4 80 7f 80
[30166.304366] mwifiex_pcie 0000:01:00.0: last_event_index = 2
[30166.309956] mwifiex_pcie 0000:01:00.0: last_event: 0b 00 0a 00 0b 00 0b 00 0a 00
[30166.317370] mwifiex_pcie 0000:01:00.0: data_sent=1 cmd_sent=1
[30166.323130] mwifiex_pcie 0000:01:00.0: ps_mode=1 ps_state=0
[30166.328788] mwifiex_pcie 0000:01:00.0: failed to get signal information
[30166.336084] mwifiex_pcie 0000:01:00.0: ===mwifiex driverinfo dump start===
[30166.337333] mwifiex_pcie 0000:01:00.0: PREP_CMD: FW is in bad state
[30166.343008] mwifiex_pcie 0000:01:00.0: info: MWIFIEX VERSION: mwifiex 1.0 (16.92.21.p84)[30166.343033] mwifiex_pcie 0000:01:00.0: PCIE register dump start
[30166.349540] mwifiex_pcie 0000:01:00.0: failed to get signal information
[30166.357569] mwifiex_pcie 0000:01:00.0: pcie scratch register:
[30166.375967] mwifiex_pcie 0000:01:00.0: reg:0xcf0, value=0xfedcba00
reg:0xcf8, value=0x4bb009e
reg:0xcfc, value=0xde00
any suggestion is welcome.
Thanks.
Hi @ArthurC
For debug purpose, is it possible load driver/FW by modprobe command refer to UM11490 as below:
modprobe moal mod_para=nxp/wifi_mod_para.conf drvdbg=0xa0037
and then catch dmesg logs from device boot with FW dump after issue occurred.
sorry for inconvenient.
Thanks.
Yao
Hello @yao_feng,
Already did it!!
There are mass logs flushed our buffer & it's hard to capture.
Is there no expert to support FW issue in NXP?
Why don't response in the post?
Hi, @ArthurC
I have to apologize to you because of any inconvenience.
This case is already dealt with by our NXP experts, but right now they request the logs as mentioned before.
According to our company support policy, our expert team doesn't communicate or post directly on our community. I am here supporting you, for some questions or issues I can answer, I will directly answer. For some firmware issue or too difficult issues I could not resolve, I will create an internal case to our expert team to ask help from them. They will support us for sure.
I know requesting logs may cause some inconvenience to you, but with requested logs, we can narrow down the issue and speed up resolution process. Sincerely hope you can understand.
Best regards,
Christine.
Hello @Christine_Li
The requested log about initialization is as attached.
It should be enough to narrow the issue cause.
For log about issue occured, please find logs provided before.
Hi, @ArthurC
Thanks for providing us again logs.
I will forward to our internal expert team to check, and once have any updates, I will let you know.
Best regards,
Christine.
Hi @Christine_Li
Customer attached related logs, please help for it.
Thanks a lot.
Yao
Hi Christine
Thanks for help, will reproduce to get dump file.
In the other hand, could you please help to analyze below hex command error meaning and any register table doc. can be shared for reference. first
[30166.275480] mwifiex_pcie 0000:01:00.0: last_cmd_id: 16 00 a4 00 16 00 a4 00 7f 00
[30166.282984] mwifiex_pcie 0000:01:00.0: last_cmd_act: 00 00 00 00 00 00 00 00 00 00
[30166.290579] mwifiex_pcie 0000:01:00.0: last_cmd_resp_index = 0
[30166.296434] mwifiex_pcie 0000:01:00.0: last_cmd_resp_id: 16 80 7f 80 16 80 a4 80 7f 80
[30166.304366] mwifiex_pcie 0000:01:00.0: last_event_index = 2
[30166.309956] mwifiex_pcie 0000:01:00.0: last_event: 0b 00 0a 00 0b 00 0b 00 0a 00
[30166.317370] mwifiex_pcie 0000:01:00.0: data_sent=1 cmd_sent=1
[30166.323130] mwifiex_pcie 0000:01:00.0: ps_mode=1 ps_state=0
[30166.357569] mwifiex_pcie 0000:01:00.0: pcie scratch register:
[30166.375967] mwifiex_pcie 0000:01:00.0: reg:0xcf0, value=0xfedcba00
reg:0xcf8, value=0x4bb009e
reg:0xcfc, value=0xde00
Thanks.
Hi, @yao_feng
Sorry, I could not explain these without our internal expert's help. These information is encapsulated in our driver and FW. I don't have permission to check. It seems like some command actions and response between Wi-Fi Card and SOC through PCIE.
According to our corporation experience, our internal expert will ask us to provide fw_dump firstly once receive any cases related to firmware crash.
Apologize again for any inconvenience to you.
Best regards,
Christine.
Hello @Christine_Li
The log about start up with time is as attached.
It should be enough with previous logs to narrow issue cause.
Hi, @ArthurC
We had a chance to work with our internal. We have prepared a test firmware to check on your platform. Can you please help to test with shared firmware?
Name : w8997_combo.bin
md5sum: 9e38158b494468cdf53ba9239ca38d84
Name : w8997o.bin
md5sum: d932dbfc38fc89d904149025d337c6a0
Version : 16.92.21.p255
If the issue is still observed by the customer please request the customer to share below mentioned logs.
I will send the test firmware to your email because here is public community. It is not good to post here.
Best regards,
Christine.
Hi, @ArthurC
Thanks for your quickly reply.
It is our pleasure to service you.
And sure, please take your time to do stress test on the new FW.
Please feel free to contact us, if still face any issue on the new FW. And also this is only a test FW for verification, if there is no problem, we will share you the official one to fix the issue you reported.
Best regards,
Christine.
Hello, @Christine_Li ,
Yes, there is.
After tested 7 days, the test result about w8997o.bin with FW Version 16.92.21.p255 is positive.
The issue is not occured anymore.
Please help to release the official format for our production.
Thank you.
Hi, @ArthurC
Can you please help to double confirm :
1. whether use same test method when you verify this issue? I mean, testing the coexist of Wi-Fi and Bluetooth?
2.Are you sure you used this FW:w8997o.bin, not w8997_combo.bin?
Because as I know, w8997_combo.bin is a Wi-Fi and Bluetooth combination firmware. But w8997o.bin is Wi-Fi only firmware.
The reason we provided these two firmware is we changed in Wi-Fi firmware so shared Wi-Fi only and combo.
I feel confused if your Bluetooth can work well with w8997o.bin.
Best regards,
Christine.
Hello @Christine_Li ,
Can you please help to double confirm :
1. whether use same test method when you verify this issue? I mean, testing the coexist of Wi-Fi and Bluetooth?
-> Yes, we use the same method to verify.
2.Are you sure you used this FW:w8997o.bin, not w8997_combo.bin?
Because as I know, w8997_combo.bin is a Wi-Fi and Bluetooth combination firmware. But w8997o.bin is Wi-Fi only firmware.
The reason we provided these two firmware is we changed in Wi-Fi firmware so shared Wi-Fi only and combo.
I feel confused if your Bluetooth can work well with w8997o.bin.
->Yes, we use w8997o.bin.
Because we need to set Bluetooth baud rate in 3M in kernel driver in stable.
uartuart8997_bt_v4.bin is from https://github.com/nxp-imx/imx-firmware/blob/lf-6.1.1_1.0.0/nxp/FwImage_8997/uartuart8997_bt_v4.bin
So we use "uartuart8997_bt_v4.bin" + "w8997o.bin" to test.
Bluetooth feature is bring-uped by https://elixir.bootlin.com/linux/v5.15.71/source/drivers/bluetooth/hci_mrvl.c
Wi-Fi feature is bring-uped by https://elixir.bootlin.com/linux/v5.15.71/source/drivers/net/wireless/marvell/mwifiex
Ported them successful by myself.
BTW, if there is a "uartuart8997_bt_v4.bin" with version matching w8997o.bin which could be provided will be prefect.
Hi, @ArthurC
Our AE team is still checking internally with R&D, once have any updates I will let you know.
And for now, you can use previous test FW for daily debugging and verification to make your project proceed. But for production, please wait for our official release. I will push our internal team to give an ETA firstly.
Best regards,
Christine.
Hello @Christine_Li ,
How is the status about new firmware releasing?
During the test in thease days, we found that the test for firmware about Wi-Fi is stable. But the Bluetooth signal is getting weak in the working situration with 2.4G Wi-Fi iperf + A2DP Audio play. Will cause disconnection often and no error logs but can be recovered by re-connection.
Please help to confirm the bluetooth firmware releasing is suitable for the released Wi-Fi firmware changing.
Thank You