602 and 612 RF mixers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

602 and 612 RF mixers

441 Views
javier_romo
Contributor I

Hello,

I am investigating the old 602 and 612 RF mixers (Gilbert cell) and try to know what are the differences. I was reading both datasheets and both seems the same except in the Icc max current where 602 draws up to 2.8mA and the 612 3.0mA. I was wondering if that could be an errata since apparently the remaining characteristics all looks the same.

Thanks,

Javi

0 Kudos
Reply
0 Replies