Operating KW36 with a 26MHz XTAL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Operating KW36 with a 26MHz XTAL

Operating KW36 with a 26MHz XTAL

By default, FRDM-KW36 board includes a 32MHz XTAL (YI) as shown in Figure 1 but there are cases where a 26MHz XTAL is needed instead of 32MHz XTAL for FRDM-KW36 or a custom KW36 board.

 

y1.png

Figure 1. 32MHz XTAL from FRDM-KW36 schematics

Wireless connectivity demos from FRDM-KW36 Sofware Development Kit are configured to run with a 32MHz XTAL by default, but it's very easy to modify the software to operate with a 26MHz XTAL.

Follow next steps to configure a FRDM-KW36 wireless connectivity demo to operate with a 26MHz XTAL:

1. In clock_config.h file, change BOARD_XTAL0_CLK_HZ define from 32000000U to 26000000U as shown in Figure 2.

 

26mh.png

Figure 2. BOARD_XTAL0_CLK_HZ define in clock_config.h

2. Add RF_OSC_26MHZ=1 line in preprocessor:

If using IAR IDE:

  • Right click on your project, then click options (Figure 3).

iar1.png

Figure 3. IAR project options

  • Go to C/C++ Compiler tab, then Preprocessor, and add RF_OSC_26MHZ=1 line in defined symbols window (Figure 4).

iar2.png

Figure 4. IAR Preprocessor

If using MCUXpresso IDE:

  • Right click on your project, select Properties, go to Settings under C/C++ Build, then Preprocessor under MCU C Compiler (Figure 5).

11.png

Figure 5. MCUXpresso Preprocessor

  • Click on add button from Defined symbols, write RF_OSC_26MHZ=1 and click OK to finish (Figure 6).

new.png

Figure 6. MCUXpresso Defined symbols

To finish, re-compile your project and it will be ready to operate with a 26MHz XTAL.

FRDM-KW36 SDK can be downloaded from the MCUXpresso webpage.

标签 (2)
标记 (3)
无评分
版本历史
最后更新:
‎10-01-2018 03:13 PM
更新人: