Dear Sir
I want to ask the workaround for e8052.
It is described at 12.3.0.2 Internal RMII reference clock in VYBRIDHDUG Rev.1.
I want to confirm the workaround based on "EXTERNAL CLOCK SOURCE" scheme.
Q1.
Can I select the CKO1 or CKO2 pin for the clock_Out pin(Fig42)?
Q2.
Are there any problem to select the PLL5 for clock source of the clock_Out(Fig42)?
Best Regards,
Eishi SHIBUSAWA,
已解决! 转到解答。
Hello,
Yes, it is possible to use one of CKOs, sourced with the PLL5, for the clock_Out.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Yes, it is possible to use one of CKOs, sourced with the PLL5, for the clock_Out.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------