IN the Reference Manual there are several places with statements like this:
RXFIFOSIZE field: The reset value depends on whether the specific UART instance supports the FIFO and on the size of
that FIFO. See the Chip Configuration details for more information on the FIFO size supported for each
UART instance.
Where is this information? I have looked in the Data Sheet, Reference Manual and the Fact sheet. In several places one can find the number of UARTS, but not the really specific information such as FIFO sizes.
Thanks.
已解决! 转到解答。
Hello Mark,
it is in Chapter 3: Chip Configuration.
Each IP (UART, SPI, DMA, ....) can support different configuration and it depends on the SoC design how it is configured. This chapter include those details.
/Jiri