Rene,
Could you confirm this is the right source file? I need to get it to a customer asap and need to make sure it is the Vybrid MFG Tool source file, not i.MX. Thanks!
Rene,
I have a customer who is having lots of issues with the Vybrid MFG Tool and would like the source code. I've downloaded the source code file you posted above, but when I open the .zip file there are files which seem to be i.MX instead of Vybrid. For instance, under the drivers folder it says iMX_BulkIO_Driver. Can you confirm this source code file is definitely for the Vybrid MFG tool?
Looks like the right stuff.
Can't compile, probably due to Visual Studio changes.
Will get that later....
Assuming we are good to go for now.
Thanks
Rene Kolarik do you have an update?
Karina
Thank you for following up.
This is an active product development project for us and we are still very interested in customizing the Vybrid Mfg Tool in order to use it in our industrial controller field service support tools/software.
Pete Lavelle
I also need it for a customer who is running MQX on both the A5 & M4.
Customer is SciCan.
SergioSolis any update?
Karina, do you have access to the source code?, I don't.
No. I dont have access.
rendy can you comment if this is able?
You can download it from the following link:
VF6xx MPUs with ARM Cortex-A5/M4 Core|Vybrid|NXP
Its under "Programmers (flash, etc)"
Hi Sergio
That is the compiled version of the MfgTool.
We are looking for the source code so that we can incorporate the MfgTool into our Windows based configuration tool for our Vybrid based Industrial controller.
I was able to download the i.MX mfgtool.v2.3.2.SRC.zip, which includes all of the source files.
So I presume that the source for the Vybrid version is also available??
Pete Lavelle
SergioSolis are you able to continue with the follow up.