Where can we download source for Vybrid Mfg Tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can we download source for Vybrid Mfg Tool?

Jump to solution
2,309 Views
petel
Contributor I

Where can we download the source code for the Vybrid Mfg Tool?

Thanx

Pete Lavelle

Labels (1)
0 Kudos
1 Solution
1,553 Views
rendy
NXP Employee
NXP Employee

Hello, here it is.

View solution in original post

14 Replies
1,554 Views
rendy
NXP Employee
NXP Employee

Hello, here it is.

1,552 Views
chetkaufman
NXP Employee
NXP Employee

Rene,

   Could you confirm this is the right source file?   I need to get it to a customer asap and need to make sure it is the Vybrid MFG Tool source file, not i.MX.   Thanks!

0 Kudos
1,552 Views
chetkaufman
NXP Employee
NXP Employee

Rene,

   I have a customer who is having lots of issues with the Vybrid MFG Tool and would like the source code.  I've downloaded the source code file you posted above, but when I open the .zip file there are files which seem to be i.MX instead of Vybrid.   For instance, under the drivers folder it says iMX_BulkIO_Driver.   Can you confirm this source code file is definitely for the Vybrid MFG tool?    

0 Kudos
1,552 Views
petel
Contributor I

Looks like the right stuff.

Can't compile, probably due to Visual Studio changes.

Will get that later....

Assuming we are good to go for now.

Thanks

0 Kudos
1,552 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Rene Kolarik do you have an update?

0 Kudos
1,552 Views
petel
Contributor I

Karina

Thank you for following up.

This is an active product development project for us and we are still very interested in customizing the Vybrid Mfg Tool in order to use it in our industrial controller field service support tools/software.

Pete Lavelle

0 Kudos
1,552 Views
JohnBirch
NXP Employee
NXP Employee

I also need it for a customer who is running MQX on both the A5 & M4.

Customer is SciCan.

0 Kudos
1,552 Views
karina_valencia
NXP Apps Support
NXP Apps Support

SergioSolis any update?

0 Kudos
1,552 Views
SergioSolis
NXP Employee
NXP Employee

Karina, do you have access to the source code?, I don't.

0 Kudos
1,552 Views
karina_valencia
NXP Apps Support
NXP Apps Support

No. I dont have access.

0 Kudos
1,553 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ can you comment if this is able?

0 Kudos
1,553 Views
SergioSolis
NXP Employee
NXP Employee

You can download it from the following link:

VF6xx MPUs with ARM Cortex-A5/M4 Core|Vybrid|NXP

Its under "Programmers (flash, etc)"

0 Kudos
1,553 Views
petel
Contributor I

Hi Sergio

That is the compiled version of the MfgTool.

We are looking for the source code so that we can incorporate the MfgTool into our Windows based configuration tool for our Vybrid based Industrial controller.

I was able to download the i.MX mfgtool.v2.3.2.SRC.zip, which includes all of the source files.

So I presume that the source for the Vybrid version is also available??

Pete Lavelle

0 Kudos
1,553 Views
karina_valencia
NXP Apps Support
NXP Apps Support

SergioSolis​ are you able to continue with the follow up.

0 Kudos