Vybrid VG Graphics - Spinning Tiger Demo on Auto EVB w/MQX GC355

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid VG Graphics - Spinning Tiger Demo on Auto EVB w/MQX GC355

跳至解决方案
5,317 次查看
billkrakar
NXP Employee
NXP Employee

Discussion area for partners and alpha customers who are working to get VG graphics going on Vybrid.

The intent is for this discussion to be populated by the Freescale internal team with the latest files, instructions, tips etc. to allow others to create a known working platform with the Spinning Tiger Demo running on the Auto EVB Rev C w/ MQX 4.0.2 and the MQX VG drivers (0.4.0 now and 0.5.0 shortly) using HW acceleration on the GC355 GPU.

标记 (5)
0 项奖励
回复
1 解答
3,980 次查看
ioseph_martinez
NXP Employee
NXP Employee

I added the uboot sources to the same extranet site http://freescale.com/livelink/livelink?func=ll&objid=226470266&objAction=browse&sort=name

In the tar file there is a binary if you want to skip the building process.

在原帖中查看解决方案

0 项奖励
回复
24 回复数
358 次查看
jasonwilliamson
Contributor II

Do you know if this procedure works with microSDHC cards, or is a pure microSD card required?

0 项奖励
回复
358 次查看
ioseph_martinez
NXP Employee
NXP Employee

Yep, it also works with SDHC, I just have here a working 4GB SDHC.

358 次查看
dirkdoerr
Contributor III

I was able to build MQX following the instructions.

It might be worth mentioning that I failed using a more recent version of the Windows Sourcery toolchain. After switching to Linux using the matching toolchain version I could build it.

But I failed building the tiger example:

I couldn't apply the patch. It failed with hunk #15 failed error message.

In the lists of include directories I see this:

$(GC3XX_ROOT)/hal/os/$(OS_TYPE)/inc


I couldn't find a matching directory.


Maybe I am using the wrong version of "vf600 OpenVG 0.4.0". I got mine from the Freescale compass extranet

0 项奖励
回复
358 次查看
dirkdoerr
Contributor III

Short update:

I used a wrong mqx path.

Now I can compile the demo

0 项奖励
回复