Unable to see LEDs change on TWR-VF65GS10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to see LEDs change on TWR-VF65GS10

跳至解决方案
1,554 次查看
Keith4DSmith
Contributor V

Took TWR-VF65GS10 board out of box. Plugged USB cable into J3, in standalone mode, no tower. Power LED is on.

As per instructions, step 5 'Tilt the Board', I don't see the LEDs change.

Try to setup a terminal program with the COM port created by the VF board, no activity on the COM port.

Try to debug a Hello word program via IAR and OSJtag, no connection found.

Jungo/Windriver, ver. 10.1.0.0 driver running. COM14 device available via OpenSDS - CDC Serial Port, version 1.1.2600.1. Drive E: TW-VF65GS is present.

If hold RESET button down while connecting to J3 and release RESET, see BOOTLOADER.

What have I not done or have done wrong?

标签 (3)
0 项奖励
1 解答
1,332 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
3 回复数
1,333 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
1,333 次查看
Keith4DSmith
Contributor V

When using IAR, one does not use PE Micro debugger, one uses the CMSIS DAP debugger.

Follow these steps as supplied by IAR.

1) disconnect the USB cable from the TWR-VF65GS10 if it has

   been connected,

2) run and install the EWARM's .\arm\drivers\pemicro\PEDrivers_install.exe,

3) press and hold the reset button of the TWR-VF65GS10 until

   you have reconnected the USB cable to its OpenSDA/Micro-USB

   connector (J3)

4) copy the EWARM's .\arm\drivers\pemicro\OpenSDA\CMSIS-DAP_OpenSDA.S19

   file into the drive E: TWR-VF65GS,

5) disconnect and reconnect the USB cable,

6) set your project's workbench menu "Project>Options>Debugger>

Setup>Driver" to "CMSIS DAP" and "Project>Options>CMSIS DAP>

JTAG/SWD>Interface" to "SWD",

This setup powers the Vybrid controller via the USB cable connected to J3.

0 项奖励
1,333 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

The Tower systems comes with a micro SD memory you have to plug into the TWR SD connector.

The SD contains the binary image. Also please make sure the jumpers are configured correctly.

Best Regards,

Alejandro