Toggling rx pin reboots linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Toggling rx pin reboots linux

1,942 Views
Rikard
Contributor I

Hi,

we have a board with a MVF61NN151CMK50 chip running Linux.

During boot some of our boards will have a Linux soft lockup before Freeing init memory, this is only when ambient temperature is above 65° C.

If the Rx pin is connected to ground, or with the FTDI USB to UART interface for debugging, we do not have this issue with the boards with temperature problems.

The Rx pin is connected to SCI0_RX.

If we disconnect the Rx pin, Linux will sometimes reboot.

What can cause the Rx pin to have soft lockup when the ambient temperature is + 65° and reboot of Linux indepnedent of temperature?

0 Kudos
Reply
0 Replies