Hi, Dear Vybrid team
I am learning the material AN4807 for Power consumption measurement.
I have a few questions for the measurement result:
1. 1. What’s the measure point for the following data? Is it 3.3V input? Or core 1.2V?
2. 2. What’s the CPU frequency for the following case?
3. 3. What’s the “reset status” meaning? Similar to “standby” status?
Many thanks
已解决! 转到解答。
Hi Liu,
1. Mentioned data are from Datasheet ver.4 and show current consumption of the core voltage 1.2V. Please note that those currents strongly depends on the application - in real they are much less - all explained in mentioned AN4807.
2. Dual Core CA5 399MHz / CM4 133MHz. Please see chapter 3, where are described selected use cases.
3. Reset state is measured when reset is active - for example when reset button is pressed.
/Jiri
Hi Liu,
1. Mentioned data are from Datasheet ver.4 and show current consumption of the core voltage 1.2V. Please note that those currents strongly depends on the application - in real they are much less - all explained in mentioned AN4807.
2. Dual Core CA5 399MHz / CM4 133MHz. Please see chapter 3, where are described selected use cases.
3. Reset state is measured when reset is active - for example when reset button is pressed.
/Jiri
Some additionall questions:
I need to extend the figures of the AN.
Lokking at the different tables, I see that 25C to 85C correspond to an increase of around 20% of the power consumption.
Then increasing the frequency of both core to 500/166MHz also increases of 20% the power consumption.
Since both have a mutual effect, and taking the Linux power consumption, I made the following extension.
For the cores at 25C 399/133 266mA should become 1.2x1.2x266=383mA at 85C 500/166.
My customer requested more accurate figures.
May we also specifiy more or less what each and every IP would consum under various operating conditions (Temp, Freq). Simulation values would be enough.
May we provide those data?
Hi Rodrigue,
in AN chapter 7.3 is table on temperature measurements. Also document on community vybrid_current_measurement_jiri.xlsx list 9.
it shows that different between 25 and 85°C is 36%.
Between 400 and 500MHz is 20%.
Hopefully it will help you. There is also document with simulations - but it is not public.
/Jiri
Hi Rodrigue,
it is not public. Placed in Vybrid FAE space.DieSizeEstimation_Power_RunIDD_LKG_calculator_Sheet_V11_17May2012.xlsx
/Jiri