Some additionall questions:
I need to extend the figures of the AN.
Lokking at the different tables, I see that 25C to 85C correspond to an increase of around 20% of the power consumption.
Then increasing the frequency of both core to 500/166MHz also increases of 20% the power consumption.
Since both have a mutual effect, and taking the Linux power consumption, I made the following extension.
For the cores at 25C 399/133 266mA should become 1.2x1.2x266=383mA at 85C 500/166.
My customer requested more accurate figures.
May we also specifiy more or less what each and every IP would consum under various operating conditions (Temp, Freq). Simulation values would be enough.
May we provide those data?