Does Freescale have a UBOOT and LTIB source & binaries that can be used for a demo / demos?
Any issues known using CentOS Linux as host Linux?
I am looking for a non TImeSYS based version of UBOOT AND LTIB.
Will the Automotive Vybrid platform and UBOOT be available?
If not, can I get access to the final schematics/layout files and UBoot as an alternative to Tower board?
Phytec board is possible alternative and I am evaluating at present.
已解决! 转到解答。
Emcraft Systems will support U-boot and Linux for the Vybrid VF5 and VF6 devices. Software distribution is available from Emcraft's web site at registration:
www.emcraft.com/som/vf6#software
The hardware plartform is the Emcraft VF6 System-On-Module, using a Tower-compatible development baseboard:
Hi Terry,
I can only answer for the u-boot questions; sorry.
Last time I checked the support for Vybrid had not made it to DENX "mainline" u-boot but it was already in the imx "custodian" tree:
git://git.denx.de/u-boot-imx.git
(master branch)
The config you want is vf610twr.
Best regards,
V.