How to setting for the Control Register 137 (DDRMC_CR137)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to setting for the Control Register 137 (DDRMC_CR137)

Jump to solution
531 Views
keisukewatanabe
Contributor III

Dear support,

area : 19–16 PHYCTL_DL

Please tell me how to set this register.

After Leveling, and is set automatically?

Best regards,

Keisuke Watanabe

Labels (1)
0 Kudos
1 Solution
420 Views
ioseph_martinez
NXP Employee
NXP Employee

Hi Keisuke,

this is related to clock de-assertion and assertion, like when you go to low power modes.

So, The timing for sending the power-down or self-refresh command and the timing for disabling the clock are independent and unrelated, and therefore a situation could occur in which the clock is disabled before the power-down or self-refresh command has been sent. This could be catastrophic for memory data

So for this parameter, consider if you are using low power modes where you need your memory to be kept on self refresh mode. If yes, you need to check how many cycles are required for sending a self-refresh command or a power-down command and use that timing.

View solution in original post

0 Kudos
1 Reply
421 Views
ioseph_martinez
NXP Employee
NXP Employee

Hi Keisuke,

this is related to clock de-assertion and assertion, like when you go to low power modes.

So, The timing for sending the power-down or self-refresh command and the timing for disabling the clock are independent and unrelated, and therefore a situation could occur in which the clock is disabled before the power-down or self-refresh command has been sent. This could be catastrophic for memory data

So for this parameter, consider if you are using low power modes where you need your memory to be kept on self refresh mode. If yes, you need to check how many cycles are required for sending a self-refresh command or a power-down command and use that timing.

0 Kudos