From MQX to Baremetal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

From MQX to Baremetal

1,002件の閲覧回数
SlaveToTime
Contributor II

Hi,

I'm trying to do something complicated.

I have code written for Crossworks,a Baremetal project for M4.

I don't need,and probably it should be only a complication, to use MQX.

The only problem with this is that the MCC and examples,are written only for LINUX(A5)/MQX(M4), or MQX(A5)/MQX(M4).

I am only interested to not change the MCC part on linux,if it is possible,but only the MQX part of MCC.

Do you think that it is possible and not so complex?

What's the best way in your opinion?

ラベル(5)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

689件の閲覧回数
timesyssupport
Senior Contributor II

Hello Alessandro,

It should be possible to port MCC to another RTOS; however, I cannot say the exact amount of time it would take, as Timesys has not used the Crossworks baremetal project.

We would imagine the MCC sources for MQX would be the best starting point. These are located in your MQX installation directory, at mcc/source/.

We also have an MCC User Guide available at the following location, which has more information about the MCC API and implementation:

https://linuxlink.timesys.com/docs/wiki/engineering/userguide_vybrid_mcc

Thanks,

Timesys Support.

689件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help to attend this case?

0 件の賞賛
返信