Disable the SGI.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,526件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer would like to disable the SGI.

In the current Integrity OS, SGI( Software-generated Interrupts) is enabled by default.

For SGI is not used in customer system, we want to disable.

Would you advice should be disabled in any such a procedure?

If you have any sample software I think want me to reference.

ラベル(1)
0 件の賞賛
1 解決策
1,145件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
5 返答(返信)
1,146件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
1,147件の閲覧回数
takashitakahash
Contributor III


Hello Jiri-san

Thank you for your information.

I talk to with taku-sann GIC settings.

Thank you,

Best.

T.Takahashi.

1,147件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi,

this looks like a question for Green Hills (developer of INTEGRITY RTOS).

Regards

Rene

0 件の賞賛
1,147件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ what is the next step here?

0 件の賞賛
1,147件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

this has  been discussed with Taku-san. It is depended on design of SoC (based on implementation or ARM GIC). It is not possible to disable SGI separately.

You can

- disable all interrupts or

- do not assert software interrupts

/Jiri

P.S. discussed internally here  Vybrid SGI implementation and SGI configuration on Vybrid