Hello all,
I am looking for a microcontroller with large on-chip SRAM. My application includes 2-3 SPI devices, 25-30 GPIOs, 3 timers and a Ethernet based TCP/IP connection.
And I came across Vybrid VF3xx series microcontroller which has 1.5 MB of SRAM with SPI and Ethernet as peripherals.(Exactly what I wanted..!!)
Most of the support/discussions I saw were for real time operating systems, and I don't need a RTOS for my application, so is it possible to do simple bare metal C coding on this device?
Are there drivers available which will help me quickly interface SPI, GPIO, Ethernet and timers without using RTOS?
Is there any library for TCP/IP stack which can be used without RTOS on this device?
Also is it possible to do a Ethernet firmware update on this device?
I am new to this so please correct me if I have asked a silly question.
Thank you.
Chinmay
已解决! 转到解答。
Hi,
The closest thing we have in baremetal is the next sample projects:
Sample Code for Vybrid Controller Tower System
The examples are developed for the vybrid twr system. But it should be easy to migrate those projects.
Best Regards,
Alejandro
Hi,
The closest thing we have in baremetal is the next sample projects:
Sample Code for Vybrid Controller Tower System
The examples are developed for the vybrid twr system. But it should be easy to migrate those projects.
Best Regards,
Alejandro