Bare metal C coding for VF3xx series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bare metal C coding for VF3xx series

Jump to solution
1,415 Views
chinmay_a
Contributor I

Hello all,

I am looking for a microcontroller with large on-chip SRAM. My application includes 2-3 SPI devices, 25-30 GPIOs, 3 timers and a Ethernet based TCP/IP connection.

And I came across Vybrid VF3xx series microcontroller which has 1.5 MB of SRAM with SPI and Ethernet as peripherals.(Exactly what I wanted..!!)

Most of the support/discussions I saw were for real time operating systems, and I don't need a RTOS for my application, so is it possible to do simple bare metal C coding on this device?

Are there drivers available which will help me quickly interface SPI, GPIO, Ethernet and timers without using RTOS?

Is there any library for TCP/IP stack which can be used without RTOS on this device?

Also is it possible to do a Ethernet firmware update on this device?

I am new to this so please correct me if I have asked a silly question.

Thank you.

Chinmay

Labels (3)
0 Kudos
Reply
1 Solution
1,151 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

The closest thing we have in baremetal is the next  sample projects:

Sample Code for Vybrid Controller Tower System

The examples are developed for the vybrid twr system. But it should be easy to migrate those projects.

Best Regards,

Alejandro

View solution in original post

0 Kudos
Reply
1 Reply
1,152 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

The closest thing we have in baremetal is the next  sample projects:

Sample Code for Vybrid Controller Tower System

The examples are developed for the vybrid twr system. But it should be easy to migrate those projects.

Best Regards,

Alejandro

0 Kudos
Reply