@Richard Stulens
Hi Richard,
With the Cascon tool from Göpel electronic I can program an external EEProm (M95256WMN6).
But it seems, that the BSDL File which I found ("Vybrid F Series 364MAPBGA BSDL Silicon Revision 1.1") is does not to 100% compatible to the VF5xxR Controller.
--------------------------------------------------------------------------------------------------------------------------------------------------------
I urgently need a BSDL file because an EEProm should to be programmed via the SVF512R3K1CMK4 (VF5xxR) controller.
See also my question Chip doesn't seem to work correctly with this BSDL files "Vybrid F Series 364MAPBGA BSDL Silicon Rev... .
--------------------------------------------------------------------------------------------------------------------------------------------------------
Can you help me?
Best Regards,
Andreas
已解决! 转到解答。