ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
TFC2015 UCDavis Team Chucksgon Final Report Thanks for sharing Lance Halsted​
記事全体を表示
Compilation of views taken during The Freescale Cup 2015 Worldwide Finals held at the Fraunhofer IIS during the event opening. Credit: Fraunhofer IIS
記事全体を表示
Find complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
A tomada inteligente segue a filosofia proposta pelo protocolo internacional de medição e verificação (PIMVP) que diz “não gerenciamos aquilo que não medimos”. Porém, nem sempre temos um equipamento acessível ou recurso adequado para isso. A proposta da tomada é fornecer aos usuários um sistema de medição e controle sem a necessidade de grandes investimentos. O adaptador de tomada inteligente possui um circuito de medição de corrente elétrica e um circuito para medição da tensão elétrica presente na tomada. Estas informações são, inicialmente, armazenadas em na memória interna da tomada. Um aplicativo desenvolvido para dispositivos Android se comunica com a tomada, através da rede wireless da residência. Link do dropbox para acessar arquivos: Dropbox - Tomada Inteligente
記事全体を表示
Many companies run the risk of animals such as rats and variety of insects invading plants or warehouses, where the products are liable to be contaminated, mainly food industry companies. For the above, we come up with the development of the “pest control using Freescale” which consists of implementing an electronic device that emits ultrasonic frequencies ranging from 30KHz to 65KHz generated by the FRDM KL25Z board transmitted by a buzzer and through an interface may change the operation time of our prototype. Therefore purpose of this project is to solve the pest problem in a "green way" to avoid damaging the environment. Original Attachment has been moved to: Pest_control_using_Freescale.rar
記事全体を表示
Updated: May 7, 2013 - Added 6 new chapters Author(s): Ken Hsu, Rochester Institute of Technology Dan Cheung, Rochester Institute of Technology Sam Skalicky, Rochester Institute of Technology Overview Written using the TWR-K40N512. Most of the knowledge is transferable to any of the Kinetis K family of devices. The Freescale Tower System is a modular development platform that allows rapid prototyping and re-use through interchangeable modules. A few of the modules are serial modules for Ethernet and other serial interfaces, wireless modules, audio modules, and blank proto-boards to build your own circuit. CodeWarrior 10.1 Integrated Development Environment (IDE) is a new version of CodeWarrior based on the Eclipse IDE. It provides features such as instruction level debugging, disassembly, access to device registers while debugging, processor expert, and more. It is designed to be used with Freescale’s latest microcontrollers. Modules Introduction General Purpose I/O Multipurpose Clock Generator Interrupts and Timers Serial I/O I2C Digital to Analog Converter Analog to Digital Converter Analog to Digital Interrupts Flex Timer Module Real Time Clock Cyclic Redundancy Check (CRC) Digital Signal Processing (DSP)  [Draft State] Capacitive Touch Complete course files restricted to verified faculty only.  Available for download in the Faculty-Portal
記事全体を表示
Watch the video highlights of the Freescale Cup Worldwide Finals 2015 for the training sessions. Credit: Fraunhofer IIS
記事全体を表示
Nosotros creemos que es más importante el “porque lo hacemos” a el “que hacemos” por eso nos enfocamos a un proyecto centrado a pacientes con parálisis cerebral. Tratamos de establecer un medio más cómodo y fácil de usar. Planeamos lograr nuestro objetivo con “Sen-Silla” una silla móvil manipulada por sensores y con esto lograr desplazarse de una manera más accesible a sus capacidades.         Sensilla - YouTube
記事全体を表示
El presente proyecto busca solucionar de una manera práctica y divertida actividades de terapia que pueden ser parte de la vida de cada persona con necesidades especiales, especialmente infantes. Por medio de este proyecto se pretende desarrollar la memoria y el orden lógico. Utilizando un sensor óptico para la lectura de pequeños Cubos de colores, el carro donde será transportado el sensor óptico emitirá una nota musical, misma que dependerá del color del cubo. El equipo de trabajo está conformado por cuatro   estudiantes del Tecnologíco de M
記事全体を表示
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Kate Fischl
記事全体を表示
After formal competition finished in East China, we gave a challenge and asked teams to try a hill with >30 angle, some cars successes
記事全体を表示
Find complete materials at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Entrenamiento acerca de NVIC basado en la familia Kinetis L. Para el material completo visita: https://community.freescale.com/docs/DOC-95205
記事全体を表示
A peek at where vehicle technology is headed.
記事全体を表示
Couple of new videos. This time I am running the FRDM-TFC library demo code written by Eli Hughes without any change at all-- successfully on my car. I have had the 0 ohm R24 res replaced with a higher one thanks to the soldering skills of David DiCarlo! The first video highlights demo modes 0 through 3: Car demos - YouTube Demo 0- test buttons and switches Demo 1- test servo Demo 2- test motors Second, I was able to get my little o-scope (xprotolab) to capture the camera analog out-- here: Camera testing - YouTube No major coding done but I understand the library and ports on the boards much better now.   Still haven't resolved the 'whining' apparent when I enable the H-bridge but I will try a few things this week-- it is possible it is harmless. Next steps, buffering camera data then on to control loops! Daniel Oh, I was also able to get the serial port working while code was running so I could get some dynamic feedback. This document was generated from the following discussion: Videos testing out Freescale Cup kit
記事全体を表示
La descripción de este proyecto consta principalmente de tres elementos que destacan el primero y el cual es tomado como planta principal es un reloj despertador el cual esta conformado por un freedom, un LCD de 16x2 caract. y por una pequeña bocina, este será controlado para su funcionamiento con el módulo touch del micro-controlador; como segundo apartado se tiene una tira de LEDS que se empotra a la cabecera de la cama la cual contendrá un dimmer para controlar la cantidad de luz, teniendo como máxima intensidad la hora fijada en la alarma (como apoyo además de la bocina para lograr despertar) y por último un interruptor de apagado que se pretende colocar al otro lado de la habitación donde se desee incorporar el despertador, el cual tendrá forma de canasta de baloncesto, para que solamente al anotar una canasta sea la única forma de apagar la alarma y este proceso sea interactivo. Original Attachment has been moved to: fcup.zip
記事全体を表示
Este es un teclado que tiene como propósito ayudar a las personas con problemas motrices, específicamente en las manos. Existen programas de diseño como photoshop o autocad en los cuales se puede ahorrar tiempo usando los macros con el teclado en lugar de usar el mouse para todo. KES tiene el propósito de ayudar a hacer más rápido el uso de estos programas y también ayudar a las personas con problemas motrices ya que con solo pulsar un botón será lo mismo que utilizar una combinación de los mismos. KES tiene la misión de agilizar el uso de macros en programas que conviene, aparte de el apoyo ofrecido a las personas con dificultades motrices. Enlace al video KES - YouTube
記事全体を表示
El proyecto se trata de un tiro al blanco que funciona con una pistola que emite luz infrarroja, la cual es captada por los sensores infrarrojos localizados en el centro de los blancos. De atinarle al blanco, este se esconderá y aparecerá uno nuevo.
記事全体を表示