Powertrain & Electrification: Analog and Interface Solutions for Automotive Applications

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Powertrain & Electrification: Analog and Interface Solutions for Automotive Applications

Powertrain & Electrification: Analog and Interface Solutions for Automotive Applications

In automotive applications, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems and the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators, and GPIO expanders are often used to bridge between the interconnects on the board. Also, LED Controllers, LCD Drivers and Real Time Clocks are used for interfacing between the system and user. In this session, we will explore the application of these analog and interface devices from NXP and discuss their applications in automotive applications.

标签 (1)
附件
无评分
版本历史
最后更新:
‎10-14-2019 02:55 PM
更新人: