whether roll-over time need to consider in the Global timer base count value?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

whether roll-over time need to consider in the Global timer base count value?

ソリューションへジャンプ
1,934件の閲覧回数
karunakaranradh
Contributor IV

We are using T2080 based processor board. processor are operating by the below mention frequency.

System Clock is 100Mhz

Platform Clock is 500Mhz

MPIC Clock is 250Mhz

Global Timer is 31.25Mhz (MPIC is the clock source for timer, Prescaler is 1/8).

  Time Count for 1sec = 31250000 (decimal)

  Time Count for 1msec = 31250 (decimal)

I am setting  the 31250 (decimal) value in Global timer base count register (MPIC_GTBCRAn) to configure 1 mili sec timeout and roll-over condition is configured as "GTCCRxn is reloaded with the GTBCRxn value" in the MPIC_TCRn.

Global Timer is running for 3min by the external timer and check the interrupt count. the expected counts is 180000 tolerance may be +/- 1. but only 179994 interrupt counts occurred. Six interrupt counts is missing  i.e 6 msec drift is there with that 1msec count value running fro 3 min.

After i changed the base count value from 31250 to 31249 (consider the roll-over time), with this one count less we got the expected 180000 interrupt counts.

(Note: external timer already verified with scope.)

whether roll-over time need to consider in the Global timer base count value?

or

How to manage the clock drift?

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
1,581件の閲覧回数
r8070z
NXP Employee
NXP Employee

The counter states for one clock cycle (t_clk) for each count value. The start count value is the base count value (N). The last count value is 0. After the last state count is repeated in the same way from N to 0. So for each timer period (T_tmr) counter goes through N, N-1, … 1, 0 states and that takes (N+1) clock cycles. Correspondingly

T_tmr = (N+1) * t_clk

  It is the same as length of zero-based indexed array. Total number of the array elements is max_index +1. Because there is array element with index 0 in additional to 1, 2 ... max_index elements.

Unfortunately I could not find any app. note for the MPIC global timer.

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
1,581件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

 

Global Timer toggle interval is equal to (base_count_register_value + 1)*clock_period.

Hence for 3 min we shoud get 179994 interrupt counts because of 31250000*(3*60)/(31250+1)= 179994,2402

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
1,581件の閲覧回数
karunakaranradh
Contributor IV

Hi Serguei Podiatchev,

Thanks for your reply.

If i calculated base count for timeout period in msec.

base count = (freq in Hz / 1000) * (timeout period in msec)

e.g: For calculate base count for 10 msec timer timeout value  is  [((31250000 / 1000 ) * 10) = 312500]

As per your statement, I assumed the base count register value is entered as 312500 for 10msec.

Global Timer timeout interval =  (312500 + 1) * 32 nano sec = 10000032 nano sec

i.e) 32nano sec drift will added in every timeout interval.

Why to add plus one with base count register value to calculate Global Timer toggle interval?

I referred other global timer in reference manuals like MPC107, MPC8641D and P1022 processor which is identical to T2080 global timer, no where i found this formula.

This formula is applicable only for T2080 processor other processor or memory controller also which i mention above freescale product.

Is there any application notes is available for calculate the base count value ?

Regards

Karunakaran R

0 件の賞賛
1,582件の閲覧回数
r8070z
NXP Employee
NXP Employee

The counter states for one clock cycle (t_clk) for each count value. The start count value is the base count value (N). The last count value is 0. After the last state count is repeated in the same way from N to 0. So for each timer period (T_tmr) counter goes through N, N-1, … 1, 0 states and that takes (N+1) clock cycles. Correspondingly

T_tmr = (N+1) * t_clk

  It is the same as length of zero-based indexed array. Total number of the array elements is max_index +1. Because there is array element with index 0 in additional to 1, 2 ... max_index elements.

Unfortunately I could not find any app. note for the MPIC global timer.

0 件の賞賛
1,581件の閲覧回数
karunakaranradh
Contributor IV

Hi Serguei Podiatchev,

Thanks for your information.

Based on your information,I understand Base count register(MPIC_GTBCRAn) value is set it to 0 for generate interrupt in every clock cycle (i.e 32nano sec).

MPIC_GTBCRAn    Timeout Time(nano sec)

0                              32

1                              64

10                            352

31250                      1000032

31250000                1000000032

As per the formula (T_tmr = (N+1) * t_clk), I have to set the base count register with one count less to get the accurate timer out value of the timer.

But I still have doubts, I referred another (P1022) QorIQ  processor reference manual  since t2080 processor reference manual does not have example base count value for global timer.

The below example snap shot is taken from the Document Number: P1022RM Rev. 2, 04/2013,  section : 10.3.19 Timer control register group n (PIC_TCRn)

pastedImage_2.png

The above example is configured for 1hr in cascaded mode. In that Timer0 count value is calculated as 1 sec based on that 41.625Mhz frequency(i.e 0x27B_25A8 value is calculated for 1sec).

Is the P1022 processor global timer also applicable for the same formula to calculate the base count register?, If it is applicable, the timer 0 is configured for 1sec + 24 nano second. this lead to 86 micro second time drift per hour.

0 件の賞賛