what is the power consumption of T2080 in sungle core mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the power consumption of T2080 in sungle core mode?

1,064件の閲覧回数
ilanwittenberg
Contributor I

what is the power consumption of T2080 in sungle core mode?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

677件の閲覧回数
ufedor
NXP Employee
NXP Employee

Example for one core of the T2080 running at 1533/600/1867MHz with Altivec  power-gated off:

1) from the Table 6. T2080 power dissipation with Altivec power-gated off we have the VDD +SVDD  power consumption at 105C is 17.2W

2) savings for one core (PH10, PH15, PH20) are provided in the Table 10. T2080 Rev 1.1 single core/single cluster low-power mode power savings, 1.0 V 105C

3) overall (three cores powered off):

17.2 - (PH10 + PH15 + PH20) * 3 = 17.2 - (0.82 + 0.23 + 0.35) *3 = 17.2 - 4.2 = 13W

0 件の賞賛
返信