i have loaded a new image fsl-image -core changing conf to add gcc,make etc
and the file size is big
when i load the file the file shows that the file
error fs ext2 :u image cannot be defined 10755 fsl-image minimal
and also showing
error at stack 0x701 iam not able to boot my system
please help
Do you use the ext2.gz.u- boot file of the fsl-mage-core file system?
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Try to use fsl-image-full for your changing.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------