t4240 linux irq affinity to use for multiple cores

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

t4240 linux irq affinity to use for multiple cores

1,458 Views
sedataltun
Contributor I

Hi all,

We are using custom board based on t4240rdb (SDK V1.6) and want to distribute pci express interrupt to all cpu cores to make load balancing.

Pci express works in legacy mode. irq number is 40.

"/proc/irq/40/smp_affinity" value is "ffffff".

But, unfortunately, pci interrupt always processed in one core* with this configuration setting. When we change smp_affinity value for some specific cpu core it works fine, but it is not possible to work with multiple cores.

What could be the reason? How should be distributed pcie interrupt for all cpu cores?

*pci irq core number starts with CPU0, after resetting smp_affinity to ffffff again, it arbitrarily changing to other cores.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,119 Views
scottwood
NXP Employee
NXP Employee

The interrupt controller on t4240 does not support this, nor is it desirable behavior due to cache locality.  If you're going to set IRQ affinity manually, the IRQ affinity should be set to a CPU in the same cluster as the CPUs that interact the most with the device, and try to avoid assigning multiple high-workload interrupts to the same CPU.

0 Kudos
Reply