input clock DIFF_SYSCLK/DIFF_SYSCLK_B common mode requirements - T1042 Data sheet discrepancy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

input clock DIFF_SYSCLK/DIFF_SYSCLK_B common mode requirements - T1042 Data sheet discrepancy

260 Views
trevorfox
Contributor II

T1042 data sheet specifies a common mode of the DIFF_SYSCLK/DIFF_SYSCLK_B inputs as required to be 100 mV - 400 mV per section 3.22.2.3

However, the section 3.6.6 has a "receiver reference diagram of the Differential System clock" and shows an LVDS input buffering.

LVDS has typical common mode range of 1 - 1.2V, but T1042 specifies the common mode range of input clock to be 100 mV - 400 mV. 

What is that standard that the DIFF_SYSCLK/DIFF_SYSCLK_B should be following? If the external clock is LVDS, what is proper way to terminate it for the T1042 since it seems to have an off common mode range requirement? Are AC coupling caps okay?

0 Kudos
Reply
1 Reply

188 Views
yipingwang
NXP TechSupport
NXP TechSupport
Please refer T1024 datasheet for the common mode specs of DIFF_SYSCLK T1042 datasheet is due to be updated.
0 Kudos
Reply