I have a custom board with T2080 and it is interfaced with 88E1512 marvell PHY.
After dumping the uboot code,i connected the board to a PC/system through ethernet cable. Pinging and tftp works fine for 10 and 100Mbps. For 1Gpbs, the board pings 3-4 times successfully and then again goes for autonegotiTION (THIS I HAVE seen in the PC/system to which the custom board is connected). And then pings for 3-4 times and then fails to ping and again goes for autonegotiation. And coz of this, i am not able to do tftp any file at 1Gbps.
CAn anyone tell me if it is HArdware or software reason?
MOreover, in the staTUS register it shows-
Both False carrier and symbol errors being reported for 1Gbps.
Is it hardware or software in uboot issue?? has anyone faced any issue with marvel phy 88e1512?
已解决! 转到解答。
You can read some diagnose registers and understand the error where it caused from.
In PHY side you can check the register:
When you are in auto-neg mode, you need to see "resolved" in this register after 2-3 seconds. Apperently your system starting auto-neg again and again. Please make sure you have right Page 0, Register 0 configuration and not called: "Restart Copper Auto-Negotiation"
Hello,
Is the issue reproducible on another board?, it looks more like a hardware issue please provide more information and review the processor connection schematics according to the PHY datasheet, there could be a lot of reasons for example a wrong resistance value on a pin on PHY.