Whether ethernet FMAN and DPAA driver will work in latest kernel 4.20 and above?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether ethernet FMAN and DPAA driver will work in latest kernel 4.20 and above?

914件の閲覧回数
karunakaranradh
Contributor IV

We are using new microsemi VSC8575 phy in our T2080 custom processor board. New VSC8575 PHY chip family driver support is  only available from Linux kernel 4.20 and above. Currently SDK kernel (4.1.8) does not support this VSC8575 PHY driver.

Is there any updated SDK kernel version is available to support VSC8575 PHY driver ?

Is there any ethernet FMAN and DPAA driver issue will arise while using the latest kernel (4.20  and above)?

ラベル(1)
0 件の賞賛
返信
1 返信

763件の閲覧回数
carljones
Contributor III

Hi karunakaranradhakrishnan‌, were you able to make the VSC8575 chip work with FMAN and DPAA in NXP SDK? Regards.

0 件の賞賛
返信