T4240: CPU ID: Is there any way to mark the CPU if there are more than one T4240 on the board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240: CPU ID: Is there any way to mark the CPU if there are more than one T4240 on the board?

529 Views
carlpeng
Contributor II

Hello,

If there are more than one T4240 CPU on the board, are there some ways to distinguish the T4240, for example, are there reset pins to configure the order of the T4240 CPU, and after power on, can read the configured ID through reading a register in the OS?

Thank you,

Carl

Labels (1)
0 Kudos
1 Reply

411 Views
ufedor
NXP Employee
NXP Employee

It is possible.

Please refer to the QorIQ T4240 Reference Manual, 4.6.3.2 General-purpose input.

0 Kudos